This issue of The Synchrophasor Report (TSR) covers accurate timing—one of the key technologies that make synchronized phasor measurements possible. As you know, synchrophasor measurements require a precise, absolute time reference. The IEEE C37.118-2005 synchrophasor standard specifies that a clock be accurate to better than 1 microsecond. This is to ensure that the total vector error (TVE) measured by a phasor measurement unit (PMU) is less than 1 percent. There are several clocks that provide this level of accuracy, including rubidium and cesium atomic clocks; however, they are expensive and sensitive to temperature and vibration. An alternative is to implement highly accurate reference clocks, such as the SEL-2401, SEL-2404, or SEL-2407®, which are satellite-assisted clocks that use the Global Positioning System (GPS) as their absolute reference.