|
| SEL Relay Test Rack |
| |
|
Welcome to the SEL Relay Test Rack. Connect
to real SEL relays from any computer that supports TELNET communications.
When you click on the Telnet links below, your web browser will start a "Telnet" session to
an SEL Communications Processor. Through the
communications processor, you will be able to connect to
one of several different SEL
relays, listed below.
NOTE: If you are using Internet Explorer 7 or Windows Vista, you will need to work with your IT group to enable or install TELNET on your computer.
|
|
- To Login, type acc at the prompt.
- Type help for a list of commands
- Type who to see a list of relays attached to the rack.
- To exit out of a relay and return to the 2030 prompt, just press the "Ctrl" & "D" keys at the same time.
- To end your session, just close the telnet window, or type quit.
|
Click on the links below to connect to Relay Rack 1 or Relay Rack 2.
| rack1.selinc.com |
rack2.selinc.com |
|
SEL-311C
SEL-311B
SEL-387A
SEL-351S
SEL-351-7
SEL-351A
SEL-387
SEL-387E
SEL-421
SEL-300G
SEL-701
SEL-311L
SEL-2431
SEL-487B
SEL-651R
SEL-2100
|
SEL-587
SEL-321
SEL-451-2
SEL-749M
SEL-387
SEL-587Z*
SEL-501*
SEL-2030
SEL-551*
SEL-734
SEL-2411
SEL-2020
SEL-710
SEL-352
SEL-351R
|
|
|
*Passwords are set for the 500 series relays on the relay rack. For Access Level 1, the password is SEL. For Access Level 2, the password is the model number for that relay. For example, Access Level 2 password for the SEL-587Z is 587Z.
If you choose not to enter the relay rack, have problems or just want to give a comment,
please fill out the relay rack comment form. |
|

2350 NE Hopkins Court - Pullman, WA 99163 – USA
Phone: +1.509.332.1890 - Fax: +1.509.332.7990
|
|