Industry:
Website:
Product:

"We originally chose the SEL-2020 Communications Processor for its flexibility and to eliminate an RFL 9660 Digital Switch. We have installed approximately five of the SEL-2020s and found that they perform the same functions as the digital switch more reliably. In addition, we are using the SEL-2020 as the interface for our SCADA system in conjunction with an RTU performing data accumulation. The RTU serves to facilitate communications with the master control center computer system.
With the use of DNP3 off port 16 of the SEL-2020, we are able to perform all of the control and metering functions using the connected relays and were able to eliminate SCADA transducers and the interposing relays. Although we are currently using the SEL-2020 in just one substation as the SCADA interface, we plan to use more SEL-2020s in future substations along with SEL-351s, SEL-387s, and SEL-501s. There is even the possibility of eliminating the RTU altogether when the new control center computer system is implemented in the future."
Val Ammer
System Protection Coordinator
Substation Operations
OGE Energy Corp.
OGE Energy Corp. is the parent company of Oklahoma Gas and Electric Company (OG&E) and Enogex, Inc. OG&E delivers electricity to more than 755,000 retail customers in Oklahoma and western Arkansas through interconnected transmission and distribution systems that span 30,000 square miles. Today, OGE Energy and its subsidiaries employ about 3,100 men and women, operate eight company-owned power plants, and boast a long and proud history of reliable service and affordable rates.